EEO#.ZMODE

Description

Sets the type of Z pulse (index pulse) an EEO generator will create.

SOURCE    
0 (default) Once per rev One Z pulse per revolution of the output. EEO#.ZOFFSET defines the position of the Z pulse within the revolution.
1 Absolute One Z pulse in the whole position range. EEO#.ZP defines the position of the Z pulse.

In EEO#.MODE 0 (A quad B), the Z pulse will be high when A and B are high.

For EEO#.MODE 1 (cw/ccw or step/dir), the width of the Z pulse is defined with EEO#.PULSEWIDTH.

When using ZMODE 0 or 1 and multi-turn or single turn absolute feedback devices, the Z pulse generated by the EEO will always be aligned with the same mechanical position of the of the primary feedback position. If you are using an incremental feedback deviceClosedA process whereby some proportion of the output signal of a system is passed (fed back) to the input. In automation, a device coupled to each motor to provide indication of the motor's shaft angle, for use in commutating the motor and controlling its speed and position then the origin of the primary feedback is not at the same mechanical position each time the drive powers up.

If you are using EEO2 on X22, there is no Z pulse hardware signal so ZMODE has no effect.

Examples

Code

To only get a Z pulse based on an absolute position value (specified by EEO#.ZP)

-->EEO1.ZMODE 1

Context

For more information see Encoder Emulation.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type Read/Write
Units N/A
Range 0 to 1
Default Value 0
Data Type Integer
See Also  
Stored in Non Volatile Memory Yes

Variants Supported

All variants are supported.